This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ21061: Capacitor on VDD pin

Part Number: BQ21061

Hello community,

I have a question regarding the BQ21061 charger IC: Is the 2.2uF capacitor on the VDD pin strictly needed if the VDD pin is not used in an application or can the capacitor be removed (or a smaller value be chosen)?

Are there any negative effects expected when the capacitor is removed?

BR,

Stephan