Other Parts Discussed in Thread: BQ25713, BQ27510-G3, GPCCHEM, BQSTUDIO
Hi,
I am trying to build a device with 2 series LiPo cell gauged and balanced with BQ40Z50 and charged with BQ25713.
I am pretty new to cell gauging (and balancing), having only some limited experience with the BQ27510-G3, so I am sorry if I am asking basic questions, because it is hard for me to read the Technical Reference Manual.
Right now I am trying to GPCCHEM to find out which CHEM_ID is the closest match.
I have shorted cell 4 and 3 (non existent) and provided the following settings to the gauge:
- CC1=0, CC0=1 -> 2 cells
- enabled TS1 and TSint
- Temperature Mode is set on TS1
- turned off Sleep in DA Configuration
- set Design Voltage to 7200
- set Term Voltage to 6000
- send GAUGE_EN, FET_EN
After that I thought I should be able to run the charge/discharge cycle for the chem id, because things like capacity should not matter for that.
1) But while charging, the OC bit gets (together witch XCHRG) and charging stops.
Did I miss any other settings important for the GPCCHEM cycle?
Why is OC occurring? Is it because the cell capacity is still set at 4400mAh?
2) Things like charge current thresholds and design capacity should not matter at this stage? Only later when I have the correct chem id and I try to run the learning cycles to update the Qmax and Ra tables for the golden image it is important, correct?
3) The gauge reports a current that is not accurate. I assume that is because of the very small voltage drop across the 1mOhm shunt. (My electronic load showing 250mA discharge while the gauge says it's 320mA).
Will that go away if I calibrate correctly? (By using the 2A described in the EVM datasheet)
I do not have a "Pack" and a charger, but one device with a charger and fixed cells combined. Will I have to do the calibration for every single PCB?
4) Could I switch to a 10mOhm shunt?
I do not think I will need that much current and maybe the error would be much smaller when having different connectors or general PCB resistance variation.
Is it possible to switch to that shunt? Can I use different setting to still report the correct mA?
Thank you so much for any help,
Dominik