Part Number: BQ4050
Hello guys,
thanks in advance for your support.
sluuaq3.pdf:
bq4050 TechnicalReference
5.2.1 BATTERY PACK REMOVED Mode/System Present Detection
5.2.1.1
System Present
PRES is sampled four times per second, and if PRES is high for 4 samples (one second), the
OperationStatus[PRES] flag is cleared. If PRES is low for 4 samples (one second), the OperationStatus
[PRES] flag is set, indicating the system is present (the battery is inserted). If the [NR] bit is set, the PRES
input is ignored and can be left floating.
I wish to decrease the 1s total sampling period to get my device started quicker. Is BQ4050 able?