Other Parts Discussed in Thread: BQ76930EVM, BQSTUDIO, BQ78350
I have Li-ion battery packs, based on the bq76930EVM design, that (after several charge/discharge cycles) need to be discharged to below 3V per cell before the charge FETs turns on and I can charge to 4.2V again. This is without the battery capacity learning cycle being performed.
Is there a way to disable battery capacity learning and only use OCV for capacity?
Or, is battery capacity learning a "must do"?
I would be happy to just put the pack on a smart charger and have charging stop when the pack voltage reached the charge voltage.