Other Parts Discussed in Thread: LM5085, LM5145
Tool/software: WEBENCH® Design Tools
Hi Experts,
I want to design a variable power supply with TPS54561(Or any other controller/topology is fine ) for one of my applications.
Input Voltage : 50<Vin<60
Output Voltage: Min Possible to 48V (Programmable)
Current: 0 to 5A.
Now the Biggest concern is the output filter and compensation. As the filter values will vary depending on the output voltage and current.
How can I design a power supply in which I can set any output voltage between o and 48V and current can vary from 0 to 5A.
Regards
Vishal