Hello, I have a related question in wanting to charge 2x 18650 batteries in parallel (3.7V, 5Ahr combined). I've looked at the suggested BQ25616 and note in the description it says "for single cell Li-Ion". Is this part actually designed for charging multiple cells in parallel, or was it selected simply because it has much higher charging capacity? In my application, charge time is not important and I am wondering if I can use more cost effective BQ21040 or BQ24040.