This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441-G1: Issue in updating soci and socf threshold checksum

Part Number: BQ27441-G1

Hi Team,

I am working on bq27441-G2 fuel gauge and have the below queries.

1) I am unable to update the checksum for the subclass discharge.

2) I am able to update the checksum for the state subclass.

below is my sequence of updating block data values.

1) unseal the device

2) enter config mode

3) Confirm CFGUPDATE mode by polling Flags() register until bit 4 is set

4) write 0x00 to 0x61 //enable block data

5) write 0x52 to datablockclass 0x3e// for state subclass

6) wirte 0x00 to 0x3f

7) read old check sum

8) read old design capacity, design energy, tapper volt, and terminal volt.

9) calculate temp_checksum

temp_checksum = (255 - old_crc - old_values ) % 256

10) write new values

11) calculate new checksum 

new_checksum = 255 - (( temp_checksum + new_values) % 256)

Now again following the same steps from 4 - 11 for discharge and opconfig subclass.

but not able to write new check_sum

do I need to perform seal and unseal between two checksums? or need to do soft-reset?

I am able to update design capacity but not able to update discharge and opconfig values.

 

Please Help

  • Hi Rakesh,

    Please make sure that both the subclass (0x3E) and block (0x3F) information are written right before you read the check-sum. After a reset (e.g. reset between writing 0x3E/3F), this may not be initialized to valid subclass/block if you read the check-sum.

    Also you can analyze the actual waveforms on SCL/SDA and make sure that all timing requirements are truly met. Maybe something is marginal.

    Are you sending the correct commands?. Please use bqStudio first and then monitor the waveforms as an example on the EVM. Then you can implement the same sequence in your host side.

    Best,