Hi eFuse team,
I'm talking with a customer about using the TPS24751 with a reverse blocking FET, like was done in the EVM and in Figure 46 of the datasheet. They have built a board and are having some unexpected behaviour, and we're trying to get to the root cause.
On the EVM, the VGS-thresh of the FET selected is 1.0 to 1.8V. Other than just copying the EVM, do we have a spec for the FET selection in terms of VGS-thresh and any other requirements?
For example, I expect the VGS-thresh of the external FET must be lower than that of the internal FET, so the internal FET is conducting during soft-start and the load is "visible".
Thanks,
Darren