This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL1431-EP: Min cathode current for regulation over temperature

Part Number: TL1431-EP

Hello,

The TL1431-EP (and non-EP version) datasheet does not specify worst-case maximum cathode current for regulation over temperature - it is only specified at 25 C (0.45 mA typ, 1.0 mA max). What is the maximum cathode current that the application design must provide in order to guarantee regulation over temperature? Any data that you can provide would be much appreciated. 

Thanks,

-Tom Joyce