Hi,
I am designing a wearable device that is to be powered by a LiPo battery. I will use a 3.3V converter for my micro-controller. However, my ADC and Op-Amp buffer will require a bipolar supply. I used the LM27762 and came up with the following design. I want to convert the 3.3V to ±2.5V.
Does this look OK or is there something I should change regarding the LM27762. I am already consulting the forum for my ADC and Op-Amp setup so those can be disregarded for now.
Let me know if there is anything to change regarding the TLV73333 as well. However, I have used that exact design successfully before.