This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS706: Supercap management an decoupling

Part Number: TPS706

Hi,

I am using TPS70633DBV.


Now the customer asks to add a 0.5F supercap to the power supply of the board which will be located between the load and the regulator.

From the component datasheet I read it is indicated not to use more than 47 uF at the output.

How do you recommend resolving this? Is there a way to decouple the regulator from the super cap?
Is there any other more suitable component that you advise us to use?

A trivial method could be putting a resistor in series between the Vout of the regulator and the supercap. What is the minimum value that can guarantee effective decoupling?

Thank you for any suggestions.

Antonio