This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576HVS-ADJ/NOPB


Dear Sir,

I am using LM2576HVS-ADJ/NOPB to power the IC UC3526DW.
Input Voltage: 24V DCLM2576HVSADJ.pdf
Output Voltage: 12 V DC
Current Max: 1A

My voltage output waveform is not clean having some switching noise observed on DSO.
Please verify my schematic attached here and suggest changes if any changes are required.

Regards
Murthy