Dear TI team,
I have a curiosity question.
Can I use UCC3895 in a PSFB converter to drive the passive to active (P->A) leg by the IC's outputs OUTC and OUTD?
The (P->A) leg should be driven by the OUTA and OUTB as according to the datasheet. The clock rise edge is sync to the OUTA and OUTB states directly, which probably indicates that
these outputs are somewhat unique and non-interchangeable.
What are the implications for low load and high load lossess in the full bridge switches if OUTC and OUTD instead is used to drive the P->A leg?
Thank you in advance!
Best regards,
RW