This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40305: circuit is not regulating correctly under load

Part Number: TPS40305

Team,

Can you please help my customer with an implementation of TPS40305:

The circuit is not regulating correctly under load. I see your WEBENCH tool for the device but it is very limited since my MOSFETs and Inductor are not in the list of components for me to substitute. Also, the WEBENCH tool will not let me select >14V for VIN despite the DS indication that VIN MAX = 20V. Any assistance you can provide with design tools or spreadsheet calculators for this device could potentially expedite my efforts in identifying the necessary circuit changes. Any help you can provide is much appreciated.

Thanks

Viktorija