hello sir
iam trying to configure GUI with stand alone IC bq79606A-Q1.
I made whole circuit according to design recomendations provided and according to EVM. I am using 6-S battery config. i connected RX , TX , GND , and connected wake up pin to VIO . i have FT2235H setup module and iam using using FT2232H to communicate between PC and BQ. i took RX TX pins from it and connected. But when i tried to open BQ STUDIO , it says the device is not detected. but i have connected it properly as per the design , and iam getting 5V at VLDO and i pulled the wake up pin high.i double checked all the grounds and connections as per design recomendations.
( when i checked the voltage at RX and TX of BQ its showing 4.94V ) & ( when i checked on FT2232H its showing 0V on both RX and TX )
May i know any other ways to debug this issue ?
( Before connecting with microcontroller , i just want to check the interface of BQ79606 in GUI , so iam using this setup )
thank you