Hi,
For our application we use a batterypack with a protection circuit. This circuit has a cut-off voltage of about 5.6V. Can the BQ25886 handle this? For instance I see that when the battery is deeply discharged to about 4.4V, the BQ25886 performs a trickle charge and after a pre-charge. But these voltages are well below the cut-off voltage of our battery pack. Can it still perform a trickle and pre-charge in the case a battery is deeply discharged due to not using it for a longer time?