Hello,
For this specific chip, I am wanting to get a corresponding DC power source (Lipo) that would fit the requirements. I am thinking about 3.7V with 4000mAh capacity. My load varies and first I see that I can output a continuous current of around 0 to 3A. For higher loads, the input voltage should not be an issue but for those that can take 3A continuous, what is the lowest input voltage to satisfy this? From reading the datasheet I belive it said 2.7V. Once it hits this what will happen to the output current.
Best,
Tristan