Hello TI,
we testing CSD13385F5T for one of our design but as per the recommended Rating it's not handling load current ..?
We are using N-channel MOSFET(CSD13385F5T) as low side driver
Input drain voltage is 5V
Input Gate voltage is 5V
Minimum expected output Power is 5W (Output voltage 5V & Output current 1A )
Load testing on Electronics load (constant current)
What i need to do to achieve the required output power, please provide related guidelines, reference design and recommandation.
thank you in advance for sharing valuable details.
Thanks,
Rahul