Dear Support Center,
I am writing to ask about the input signal of the Enable pin of TPS2561.
When there is a waveform change of EN less than or equal to Hysteresis (55 mV) in a threshold voltage range
(0.66 V to 1.1 V),is there a risk of device malfunction or unreliability?
For example, waveform that the potential drops to 1.07 V, rises to 1.12 V, and then falls to 0 V again.
reference:
SLVS930B [7.6 Electrical Characteristics]
Thank you and best regards,