This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A90: Connecting PG to VIN

Part Number: TPS7A90
Other Parts Discussed in Thread: TPS7A91,

Hello,

In my current design, We'd like to connect a pullup resistor from Power Good to VIN (A Maximum of 3.5V) rather than VOUT. I'd really appreciate some confirmation If connecting PG to VIN is allowable in the TPS7A90 (aswell as the TPS7A91, but I imagine they're the same in this regard.)

I apologize if I've missed something obvious in the parts datasheet.

Regards

Brock Curle.

IDEX

  • Hi Brock,

    Section 7.3.7 of the datasheet explains that you can use a supply other than VOUT for the pullup:

    You just need to be sure VIN is high enough that it will register as a logic-high level for the receiving device.

    Best regards,

    Nick