Tool/software: WEBENCH® Design Tools
Hello,
I'm using WEBENCH to design a LM61460-Q1 5V@6A supply. The schematic pins for the LM61460-Q1RJR in WEBENCH show a RESET_N pin which is not described in the LM61460-Q1 datasheet. I presume this pin is actually PGOOD on the actual part. I just need confirmation that this is the case and that I am using the correct model in WEBENCH.
Also, the design includes the Rff resistor (1kOhm) but does not populate Cff (no value). Since Rff and Cff are series connected, Rff is not needed if Cff is not included. Is this a problem with WEBENCH? Is Rff to be omitted from the design or is Cff to be added?
Thanks,
Jim