This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78PL114 register modification

Other Parts Discussed in Thread: BQWIZARD, BQ78PL114, BQ78PL116

I am working with the BQ78PL114EVM to develop a multi-series cell battery pack.  I have used the BQ78PL114EVM along with bqWizard to test the proto-type pack.  I am now developing a system controller.  This system controller will need to set up, monitor, and change some charge/discharge settings while the pack is in use (Among other things).  The controller will be a low power processor such as the OMAP L138.

 

The issue I am having is finding the information I need to control the BQ78PL114.  For instance, the system controller may need to change weather the system balances on discharge, or uses the superpump mode.  I see that there are registers that control these functions and that the registers are R/W.  What I can not find is the commands/sequence to write/read these registers.  I have looked at the bq78PL114S12 API and I do not see how to modify the registers directly.  I have gone through the technical reference manual and have searched your site and the web for this information.  Is there any document that explains how to access, control, and modify the BQ78PL114 directly? 

 

Also, I am looking at the BQ78PL116.  When I try to download Technical Reference Manual for the bq78PL116 (SLUU481), I get “Sorry! We couldn’t find your page”