Other Parts Discussed in Thread: TIDA-00792, GPCCEDV
Hi,
We have designed a designed a battery pack + BMS based on reference TI Design TIDA-00792 but modified+dimensioned according to our application.
Now we want to obtain matching Compensated End of Discharge Voltage (CEDV) coefficients for the specific battery profile. In our application exist an extended mode that we can consider "average high rate", in which the battery could be able to be discharged around of 2 minutes after applyng this constant average high rate.
I have read that the fastest time interval for logging *.csv data files should be higher than 5s. It means that the log file of high rate test will have around of 24 rows. Is there any problem of using such average high rate .csv file? Are there a minimum of samples/rows in *.csv files to obtain CEDV?
Moreover, we're going to perform this average high rate test with a constant resistor. It means that the current will decrease meanwhile the battery voltage is going down through the test. Is there any problem doing this high rate test with a resistor?
Thanks,
Marco.