This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: Battery management IC selection

Part Number: BQ40Z80
Other Parts Discussed in Thread: BQ40Z60, , BQ40Z50-R2, BQ40Z50

Which IC do you recommend the best, BQ40Z50-R2/3, BQ40Z60, or BQ40Z80 ?

Our system uses Li-ion 4s battery and BMS needs functions as following.
- Cell balancing
- Over/Under voltage protection
- Over charge/discharge current protection
- Fuel gauge
- JEITA profile

About BQ40Z60, 
if a cell temperature rises when charging, is this device control charging current automatically?
or does the system have to command BQ40Z60 ?

About BQ40Z50 and BQ40Z80,
do you have any recommended charger ICs with BQ40Z50 or BQ40Z80 ?