Other Parts Discussed in Thread: LM5576, LM43603
Hi,
I Want to use the LM5576/-Q1 for a new project,
Input voltage: 45-75V
Output voltage: 38V
Current: 2.4A, in ambient temperature of 85 degrees Celsius
I can't find in the datasheet a derating curve according to the ambient temperature.
Can you please help me understand how do I calculate the maximum current that this power supply can provide in different ambient temperatures?
Regards,
Shlomy