Dear support,
we have some old battery packs BQ3055 based, mostly 20P4S configuration with LiFePO4 cells. We have several on field running fine for several years already.
The issue we're experiencing now is with some shelf spare end customer units, They go in DFF error. Most of those packs battery cells are still ok.
We have different scenarios, some they reset easily sending SMB 00 > word 0057, some needs full PF reset with command SMB 62.
What we can't figure out is that some of the boards even after the above 2 methods don't reset. I even after reload the .senc FW and the golden .GG but they don't get out of the error state.
I have also tried with the 10K resistors method instead of the packs, powering the board 12V with PSU, to isolate packs issues.
Any additional idea.
Thanks, Ermanno