Other Parts Discussed in Thread: TINA-TI
SINE WAVE OUTPUT INVERTER ASSEMBLY: FULL BRIDGE MOSFET CONTROL SYSTEM
OKAY WHAT IM TRY TO FIND OUT IS THAT CAN YOU GET THE DEVICE TO PRODUCE A CLASS-D OUTPUT DRIVE SIGNAL'S . NORMALLY YOU WOULD SET THE + INPUT OF THE ERROR AMP WITH A DC REF VOLTAGE AND YOU SHOULD SEE THE OUTPUTS OF THE DEVICE AT 50% DUTY CYCLE SQ WAVE AT THE SWITCHING FREQ. NOW WHAT I WONT TO DO TO PRODUCE THE CLASS-D OUTPUT DRIVE SIGNALS S TO SET UP THE OSC TO SWITCH AT 52KHZ ARE USE A EXT CLOCK IN , SO NOW I HAVE A RAMP SIGNAL PRESENTTHEN I WILL SET THE +INPUT OF THE ERROR AMP WITH +2.5 VDC,THE - INPUT TO THE ERROR AMP IS STILL OPENNOW I SHOULD HAVE OUTPUT DRIVE SIGNALS AT 50% DUTY CYCLE NOW ON THE ERROR AMP COMP PIN #4I INPUT A LOW FREQ SINE WAVE AT LETS SAY 400HZ AND 2V PK-PK. NOW I SHOULD SEE THE OUTPUT DRIVE SIGNALS CHOPPED TO REPERENT THE SINE WAVE IN,AND THEN I CAN ADJ. THE SINE WAVE TO GET THE BEST OUTPUT SIGNAL BEFORE CLIPPING THE RAMP SIGNAL, THEN I WILL USE A PRECISION EXT. OPAMP AS THE FEEDBACK ARE ERROR AMP CONTROL WHICH IT WILL HAVE A +2.5VDC REF ON THE + INPUT OF THE EXT. AMP. THE FEEDBACK SIGNAL WILL BE A SINE WAVE INPUT THE SAME AMPLTD. AS THE SINE WAVE REF SIGNAL ON THE COMP. PIN TO SET THE FINIAL OUTPUT VOLTAGE. SO AS I LOAD THE OUT PUT IT WILL MOVE THE PHASE CHANGE TO COMPENSATE AND KEEP THE OUT TO MATCH THE SINE WAVE REF. ON THE COMP PIN.
TAKE A LOOK AT THE DATA SHEET ON PAGE #16 FUN. BLOCK DIAG. AND LET ME NO IF I'M CORRECT
THANKS YOU,
WILLIE L. MCCAIN
wmccain@mccainlab.com
561-846-0150