This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60: battery packs were being swapped around from board to board, and report 0WHr after that.

Part Number: BQ40Z60


as title writes, after replace battery pack, our Host found battery energy is 0Whr. why? do we support replacement?

Settings Configuration DA Configuration 1a hex
  • After replacement, the first time power on:

    Gauging Status: 0x0008141a Op. Status: 0x10004193 Battery status: 0x40a7
    Charging Status: 0x000300c4 Safety Alert: 0x00000000 Safety Status: 0x00000000
    Manufact status: 0x000004f8 PF Alert: 0x00000000 PF Status: 0x00000000

    Voltage: 10614 Batt pin: 10665 Power cW: 0 ACP mV: 12700
    Cell1 mV: 3576 Cell1 mA: 0 Cell1 qmax: 0 Cell1 bal time: 117
    Cell2 mV: 3565 Cell2 mA: 0 Cell2 qmax: 0 Cell2 bal time: 116
    Cell3 mV: 3474 Cell3 mA: 0 Cell3 qmax: 0 Cell3 bal time: 0

    Full Cap cWh: 0000 RSOC: 100 Ave time full: 62
    Remain Cap cWh: 0000 ASOC: 093 Ave time empty: 65535
    STATE secs: 0089 Lstatus: 0xe Update status: 0xe
    Max Error: 1 SOH: 100 SOH FCC mAh/cWh: 1136/1105

    I found the FCC is 0, so I did power cycle:

    Gauging Status: 0x0019185a Op. Status: 0x00004193 Battery status: 0x00e7
    Charging Status: 0x00010044 Safety Alert: 0x00000000 Safety Status: 0x00000000
    Manufact status: 0x000004f8 PF Alert: 0x00000000 PF Status: 0x00000000

    Voltage: 10396 Batt pin: 10448 Power cW: 0 ACP mV: 12689
    Cell1 mV: 3481 Cell1 mA: 0 Cell1 qmax: 1137 Cell1 bal time: 0
    Cell2 mV: 3482 Cell2 mA: 0 Cell2 qmax: 1136 Cell2 bal time: 0
    Cell3 mV: 3433 Cell3 mA: 0 Cell3 qmax: 1137 Cell3 bal time: 0

    Full Cap cWh: 0972 RSOC: 100 Ave time full: 65535
    Remain Cap cWh: 0972 ASOC: 094 Ave time empty: 65535
    STATE secs: 0029 Lstatus: 0xe Update status: 0xe
    Max Error: 1 SOH: 100 SOH FCC mAh/cWh: 1136/1105

    so why first time power on, the information is incorrect?

  • Hello Harry,

    So you swapped battery packs between boards, on initial power up the FCC and RemCap both report 0, then you power cycle the gauge and the FCC and RemCap are updated?

    There are some configurations you can change using the NR bit (non-removeable pack) that could affect when you remove/insert a battery.

    Can you share your .gg file so we can take a look at the parameters you have set?

    Sincerely,

    Wyatt Keller

  • Yes, you are right. And will it trigger SUV PF fault if I remove battery pack?

  • Hello Harry,

    We can take the conversation offline.

    Sincerely,

    Wyatt Keller