Normally when the system is powered by the battery, the BATDRV turns on the N-CH FET. In the application circuit the system voltage is also connected to the AC power through another FET driven by ACFET. So my question is if BQ24725A guarantees that the BATDRV turns off the battery FET during charging. I know if somehow the AC power adapter doesn't meet those strict requirement, the battery FET will be ON, which potentially connect the AC power adapter directly to the battery.