Dear TI support
Can you help check , Why I use TPS55288 PIN14( FB/INT) the function not implemented?
I use internal feedback, and external pull-up resistors, According to the function, it should be pulled down if there is a problem, but now OK work is also pulled down, please help to confirm, or point out how I need to use the abnormal function of FB/INT, I need to use this PIN to judge the working status。
Thanks !