This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ297XY : Available parts

From the datasheet of BQ29700 series, BQ297XY has OVP:  3.85V to 4.6V and UVP: 2.0V to 2.8V, But the part number not mentioned in the datasheet.

  • hi Vishnu,
    BQ297xx is not a specific part but rather shows that, for instance for OVP, the IC could support an OVP ranging from 3.85V to 4.6V. It shows the capability of the IC. We then release specific variants of this IC and these variants have part numbers with 5 digits after BQ such as BQ29706 in the device comparison table in the datasheet.