Other Parts Discussed in Thread: TPS92691
Hi,
I am using TPS92691-Q1, seeking advise for this problem
( 5 times) encounter this chip damage as well as switching MOSFET damage when I increase LED current to 3A or more.
( I increase LED current by varying pin6(IADJ) voltage using a benchtop PSU ).
( Voltage input setting to 40V )
the damage is in not immediate, but only after about 3 mins.
below are some of my buck-boost configuration
( LED max current is 4.2A , 36V forward voltage )
( input voltage range = 32 to 54.6V )
1: dimming control PWM(pin4) and DDRV(pin11) are not used
2: switching frequency is 80kHz , pin3(RT) resistor = 105K ohm
3: pin2(SS) CAP 0.047uF
5 pin5(comp) (2.26Kohm in series with 0.068uF) + parallel 750pF
6: 2 switching MOSFETs (in parrallel) using infineon BSC190N15NS3 G (Id(max)=50A, VDS = 150V )
7: switching sense resistor (at IC pin14(IS)) to Ground) = 12m ohm (1/2W)
8: Power inductor = 22uH (coilcraft MMS1210, 8.8A (Isat) )
9: LED current sense resistor = 20m ohm (1W)