Hi team,
I'm proposing the LMR33630 to my customer. Could you help with the questions below from the customer?
Here is the requirement
Vin = 23.2V to 25.8V
Vout = 5.0V
Iout = 2.8A
Fsw=400kHz(A version) or 2.1MHz(C version)
1. Regarding the external parts selection.
Could you tell me the recommended inductance and output capacitance value for each Fsw?
For the inductor, could you also provide the required value for the DC superposition rated current Isat?
2. Could you tell me the output voltage accuracy when the converter is operating in PFM mode?
Regards,
Yamaguchi