Hi!
I would like to check if the safety timer on the BQ24090 is working fine.
In the test the cell is charged and discharged at the same time (i try to keep cell voltage on 3.3V). I detected that charging did not stop after 10 hours (cell volatge was 3,3V and charging current was 600mA).
Could you explain why it happend? Why charging proces is not stopped?
Best regrads!