Other Parts Discussed in Thread: TPS65130
I need to create +5V @ 45mA and -5V at 2mA for an analog signal processing circuit. The datasheet for TPS65135RTER says that it is designed for balanced loads such as AMOLED drivers. What happens if the loads are not balanced? I can probably live with poor voltage tolerance, but might have a problem with poor load regulation. I have been unable to find a simulation tool for this part. Please advise.