Hi all
Please find a question from my customer below regarding input capacitor value.
Please comment / clarify.
Thank you and best regards
Ueli
-------------------------------------------------------------
Last time you recommended this part TPS566235RJNT for my design requirements Vin=6.9V, Vout=3.3V and Iout max = 5A.
I was using TI WEBENCH and it generated a circuit for me (see below):
So the circuit has chosen Cin=47uF (C3216X5R1E476M160AC from TDK) and I tried to work out the value of Cin using the datasheet of TPS566235RJNT with the following formula:
I first worked out the input ripple current using Equation 6: Icin(rms) = 2.49A
Then worked out Vinripple = 2.49 x 2mohm (ESR) = 0.00499V
Then substituted Vinripple and Fsw=600KHz in Equation 5, and worked out Cin(min) = 797uF
I know my calculation was wrong because 797uF seems way too large! Are you able to shed some light please?
Thanks for your support!