Hi,
I have 2 questions:
1) Is it possible to make parallel connection of multiple channels on the same device? any counterback?
2) Is it possible to make parallel connection of multiple devices?
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have 2 questions:
1) Is it possible to make parallel connection of multiple channels on the same device? any counterback?
2) Is it possible to make parallel connection of multiple devices?
thank you
Hello Adolfo,
It is possible to make parallel connection of multiple channels on the same device. For more information about paralleling channels please read:
High-Side Switches Paralleling Channels
For our higher Ron devices (100 mOhm+), such as TPSxHxx devices, you can parallel the devices; however, for our lower Ron devices, such as TPSxHBxx/TPSxHAxx families, it is not recommended.
Regards,
Kalin Burnside