Hello Guys,
Good day.
Our customer wants to confirm if this device operates in a static high output state where the high side voltage is switched to the output and left there for several minutes?
He is providing a high and low voltage to a load using this device but want to verify operation by testing it in the high state and then the low state. He would like to set the device high and measure the high power supply voltage on its output using a volt meter or oscilloscope and then set the output low and measure it.
Can he do this? set it high and measure a static high output voltage?
In addition, he sees a minimum pulse width in the datasheet but not a maximum *** width so it would seem that static operation is possible; however, there is a bootstrap capacitor to elevate the floating high side supply during a pulse and that would seem to potentially place a limit on the time the device could remain high before the floating voltage decays.
Thanks in advance!
Art