Hello,
In our application, we want to use LM5122 to drive a 500W power amplifier for short pulse (e.g. 10 ms). The power input to our system would be around 50 W. So our idea now is to put a big capacitor at the output.
When the power amplifier is working, we expect the LM5122 to go to hiccup mode. And the capacitor would discharge to provide the required power.
When the power amplifer is in idle mode, we hope LM5122 can recover from the hiccup mode to charge the capacitor.
We would like to ask if LM5122 a good choice for this application.
Can LM5122 recover from hiccup mode? In my simulation with TI-NA spice as is shown in another thread ( ) , I am not able to get LM512 recovered from Hiccup mode.
Best regards,
Bo