Dear all,
I am doing a project with the requirement configuration stated below.
| Configuration | |
| Label | Value |
| VIN | 15V |
| VOUT | 1.2V |
| OUTPUT CURRENT |
1.5A |
I use TINA simulation tool to determine the components value. Based on that, I had made some changes to the components value that is label in the schematic below with the reference from webench power designer. Then I am using TPS54260EVM-597 evaluation module (HPA597)
However, when testing the circuit, I encounter critical issue listed below:
1: Input of Cboot voltage is 7.2V and the Output of Cboot voltage is 1.12V
2: Results for switching frequency measured before the inductor is not working
Please assist where the root cause is, Your prompt reply is appreciated.