Hi team,
customer have PGATE no output issue of LM3409.
The application is : VIN=12V, output is 3s LEDs, the VF of LED is about 2.75~3.25V. they use PWM to dimming ,the frequency is 100Hz
they found that when the PWM duty cycle is set to 0.043%, Power up, the PGATE is normal have output signals. After some minutes, PGATE is high, no output.
we have below questions:
1. why the PGATE have this issue? customer use PMOS is BUK6Y24-40P, the Qc is 23nC,35nC(max), datasheet require the Qc should be less than 30nC. is that the reasone why PGATE no output?
2. customer increase the capacitor Cf between VIN and VCC from 1uF to 10uF, can solve this problem. The datasheet show if the Qc of PMOS >30nC, the Cf shoud not connect VIN.could you help give more introdcution about this. how to modifiy this circuit in customer application?
I attached customer schematic and waveform, and test result (chinese).please help to check, thanks.