We are powering BQ25895RTWT from 5V barrel connector(DC jack) ,but from datasheet we can see input current limit is based on D+/D- detection, As we are not using USB(VBUS) to power on BQ25895RTWT, in this case BQ25895RTWT will consider as unknown adapter and sets input current to 500mA as a result we cannot achieve 5A output current. Please help me on how to achieve 5A output current when there is no USB power on. Is there a setting or pullup's or pull downs needed to achieve 5A output in the absence of D+/D-enumeration? If any reference schematics for 5V barrel connector(DC jack) is available please share us at the earliest.
Adding BQ25895RTWT circuit which we have in our design for your reference, and suggest us right solution to generate 5A output current in the absence of D+/D-.
Regards,
Satish
Thanks & Regrads,
Satish