I have an application where the load is short duration high current pulses.
The peak of the pulse is circa 25ms with a tail of about 250ms. Approx 25% of the capacity drain of the pulse is in that 25ms peak.
Will the coulomb counter capture this or will I need to add some integration to the feed from the shunt?
The datasheet is somewhat sparse on details in this area.
Thanks,
Simon