Other Parts Discussed in Thread: TPS2513
My understanding is that this chip can detect USB SDP, CDP, and DCP adapter types, as well as detect certain non-standard adapters called "Divider 1," Divider 3", and "Divider 4." However, these dividers are not defined anywhere in the datasheet. I am guessing that these refer to different resistor divider configurations that can be placed between the D+ and D- pins on the adapter side. From the related thread I read:
- "If you wish to force the D+/D- detection into Divider 3, you must apply 2.0V on D+ and 2.7 V on D-. I suggest you do this by having a resistor divider from a reference voltage to GND. This reference voltage can be created from an LDO tied to SYS or BAT similar to the EVM schematic."
What about Dividers 1 and 4? Also is there any published documentation from TI that defines these terms as used by the BQ25886 datasheet? I am asking because it would be good to know what kinds of charger adapters this chip can detect. I do not plan on forcing the chip into any mode by placing dividers on the BQ25886 side.