This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61166: LED current programming

Part Number: TPS61166

Hi Sir:

The FB voltage is 0.2-V , LED current was programmed by R1 resistor. What will happened when I set the current is 120 mA and use  PWM 100 % but the panel BL module only accepts maximum current is 50 mA ? Does it damage the panel BL module ??