This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24092: Minimum charge current reduction from 50mA to 10mA

Part Number: BQ24092

I'm using the charger to charge a TLI-1530A, Tadiran lithium battery.  The issue is that the battery needs to be charged at a max of 10mA at -40C.  Is there a way to reduce the minimum charge current of the BQ24092 to 10mA?  From the datasheet the minimum is 50mA.  This design is already fielded so only a pin for pin replacement or a way to adjust the BQ24092 to 10mA would work in this case. 

Here is the schematic for the circuit. 

Thanks