This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62056: threshold of Power-Save Mode

Part Number: TPS62056
Other Parts Discussed in Thread: TPS62065

Dear Specialists,

My customer is considering TPS62065 and has a question.

I would be grateful if you could advise.

---

As a condition for entering Power-Save Mode

There was a description in the data sheet as follows.

<Excerpt from the data sheet P.11 >

" The current is 100 mA at low input voltages and up to 200 mA with maximum input voltage. "

At this time, the input voltage is 5V and output voltage is 3.3V.

In this condition,  which is the threshold current 100mA or 200mA.

I suspect it is "low input voltages" and it the threshold current is 100mA to  "Power-Save Mode".

Is this correct?

---

I appreciate your great help in advance.

Best regards,

Shinichi