Hi Team,
According to Data sheet, accuracy of TLV7530PDRVR will be ∓1%.
Customers now require ±1%
Is there any concern such as temperature dependence?
Best Regards,
Maki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
According to Data sheet, accuracy of TLV7530PDRVR will be ∓1%.
Customers now require ±1%
Is there any concern such as temperature dependence?
Best Regards,
Maki
Hi Maki,
What are the operating conditions that the customer expecting (i.e. VIN, VOUT, IOUT, TA)? Note that the +/- 1% output voltage accuracy spec is only up to 85C junction temperature and also at Iout = 1mA, so the 1% may be violated if the junction temperature is higher than 85C or the current is significantly higher than 1mA.
Best regards,
Nick