This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Battery Charger IC

Other Parts Discussed in Thread: BQ24616, BQ76930, BQ76942

Hello TI,

               I am going to design battery charger for  6S (10000mAh) Li-Polymer battery. Battery charging current should be 10A. Also require voltage monitoring and balancing features. It should have CC,CV, and temperature control mode too. if possible, we are looking for analog solution only. My queries are as per below.

Query 1 : I found that, Battery charger IC and Cell monitoring ICs are separate. Is any part available which can serve all purposes ? Please suggest.

Query 2 : Should I combine Battery charger IC (BQ24616) and Cell monitoring IC (BQ76930) for my application ? Please suggest alternate of it if any.

Query 3 : As I want analog circuit design only, please suggest any suitable cell monitoring circuit which does not require MCU.

Thanks & Regards,

Tirth Patel,

Email : p.tirth@mphibr.com