This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23882: total power budget

Part Number: TPS23882


Hi Sir,

customer want to know how do set total power budget of TPS23882? must set up I2C and control? or auto mode function?

if customer want set 2-pair to 60w, can it?

  • Hi Tommy, yes the customer must use I2C since this is a non-standard application. You can increase the policing power to 60W on one channel using the GUI for the EVM. I recommend ordering a TPS23882EVM-008. You can set the port to semi-auto mode, power up to two pair, then increase the policing power to 60W on one channel. Thanks!